AXIS#.MT.MTNEXT

Description

The motion task control word can be selected so that a following motion task is executed after a first motion task. This parameter displays which motion task should be started after the first motion task.

<any valid motion task number> Next task is set
0 There is no next task

Examples

Usage

This keyword is used to set what you would otherwise have set with AXIS#.MT.CNTL

Code

MT.MTNEXT 0 1  Will configure Motion Task 0s next task as Motion Task 1.
MT.MTNEXT 0 -1  Will configure no task following Motion Task 0.

Context

See AXIS#.MT.CNTL for more information on the argument semantics.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only Array
Units N/A
Range -1 to 31
Default Value -1
Data Type Integer
See Also  

Stored in Non-Volatile Memory

Yes

Variants Supported

Supported on all drives.